What kind of cable is needed to connect a PC to the Matrix CM9700-CC1?

Issue

What kind of cable is needed to connect a PC to the Matrix CM9700-CC1?

Product Line

Pelco Matrix

Environment

  • Windows PC
  • CM9700-CC1 most versions

Cause

Communication between devices is required.

Resolution

A null Modem cable. The cable uses pins 2 to 3, 3 to 2 and 5 straight through.