What is the default BIOS password for the Matrix CM9740-CC1 and CM9700-CC1?

Issue

Bios setting adjustments may be required, including, but not limited to:

1. Modifying the first boot device to Floppy Disk A:

2. Modifying the IRQ settings to reflect the appropriate CM9700-SER sercom card settings.

3. Modifying the IRQ settings when adding CM9700-SER-32 rocket card

Product Line

Pelco Matrix

Environment

  • CM9700-CC1 All Versions
  • CM9740-CC1 All Versions

Cause

CM9740-CC1 or CM9700 Bios is password protected.

Resolution

This password is case-sensitive

password = pelcon