What are the default CM9760-CXTA Coaxitron Translator switch settings for P protocol using 4800 baud rate?

Issue

What are the default CM9760-CXTA Coaxitron Translator switch settings for P protocol using 4800 baud rate?

Product Line

Pelco Matrix

Environment

CM9760-CXTA version A

Cause

Physical Installation

Resolution

Switch 6 turned on in the up position.

NOTE: If D protocol is used turn off switch 8 and turn on switch 3.

NOTE: When using the Spectra Dome or Esprit camera lines also turn on Switch 8 in either mode.