Will the scheduled backup feature still run while the DX4700/DX4800 Series HVRs are in live and/or playback session?

Issue

Will the scheduled backup feature still run while the DX4700/DX4800 Series HVRs are in live and/or playback session?

Product Line

Pelco Video Management

Environment

  • DX4700(HD)
  • DX4800(HD)

Cause

Will schedule back run while in live view.

Resolution

Yes. The Scheduled backup feature allows a user to program the HVR to backup video on a daily or weekly basis. Backups will run in the background while the DX4700/4800 HVRs are under normal operation.