Will the Endura DVR5300 Series digital video recorder support 1 TB (terabyte) hard drive size?

Issue

Will the Endura DVR5300 Series digital video recorder support 1 TB (terabyte) hard drive size?

Product Line

Pelco Video Management

Environment

  • DVR5300

Cause

The hard drives originally used in the DVR5300 are going obsolete and much larger drives are now available. Can the DVR5300 take advantage of those larger storage sizes?

Resolution

The maximum storage capacity that the DVR5300 will utilize is 750 GB (Gigabyte). Although a replacement hard drive size can be 1 TB, the DVR5300 will only recognize and utilize 750 GB. Therefore, if a 750 GB hard drive is unavailable, a qualified 1TB drive from Pelco can be used as the replacement drive.

Hard drive replacement part numbers:

Part # Description
HD5000-250 Replacement 250 GB drive and carrier
HD5000-500 Replacement 500 GB drive and carrier
HD5000-750 Replacement 750 GB drive and carrier
HD5000-1000 Replacement 1 TB drive and carrier