Issue
What HHC (Hand Held Console) cable do I need to connect to a DCU, UCI, or PCU?
Product Line
TAC INET
Environment
I/NET
HC7410 HHC (Handheld Console)
Cause
Can not locate documentation to indicate which cable is required.
Resolution
Original HHC: The part number is 602135-0003. It is a six foot (or 1.8 m) coiled, silver modular cable. Refer to the appropriate controller TCON for more details.
HHC (Hand Held Console) is also called the HC7410. Refer to TCON 073 for more details.
Updated USB HHC:
This is the replacement for the HHC. TCON318 has more information. The HHC-USB-IF cable allows you to connect the hand-held console (HHC) port of a TAC I/NET device to the USB port of a PC. You can then use the HHC emulator running on the PC to configure the I/NET device’s controller LAN address, tap emulation, baud rate settings, monitor and control points, and perform the other typical local maintenance functions supported by the earlier HC7410 console product.
The HHC-USB-IF cable can be used with the model 7716, 7718, 7756, 7780, 7790A, 7700, 7740, and 7750 Distributed Control Units (DCUs), and the model 7760 UCI