Can the KBD4000 function as a stand-alone keyboard such as the KBD300?

Issue

Can the KBD4000 function as a stand-alone keyboard such as the KBD300?

Product Line

Pelco Matrix

Environment

KBD4000 keyboard

Cause

The function of KBD4000 keyboard was to work with Genex Multiplexer.

Resolution

No. The KBD4000 keyboard is a full-function keyboard that must connected to a MX4000 Genex® Multiplexer or MX4000SVR Genex Multiplexer Server.