What is the default log on password for the CM8500 Matrix System?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Default Log On password for CM8500 Matrix.

Product Line

Pelco Matrix

Environment

  • CM8502A-1
  • CM8503A-1
  • CM8505D all models

Cause

Default Password

Resolution

Default password:

  1. Press the ENTER button on keyboard. At this time and on-screen keyboard will appear on the monitor screen. Refer to figure below.
  2. Using the joystick and the [point] button, Enter: [1]
  3. Using the joystick and the [point] button, Enter: [space] which is the onscreen (blank key)
  4. Using the joystick and the [point] button, Enter: [99999 Ent]