How to check the software version running on the CM97xx-CC1 Matrix.

Issue

How to check the software version running on the CM97xx-CC1

Other Symptoms may include:

  1. Software Incompatibility between CM9700-CC1 version and CM9700 System Manager
  2. CM97xx-CC1 fails to launch program after making file changes

Product Line

Pelco Video Management, Pelco Matrix

Environment

  • CM9700 Series Matrix - All Versions
  • CM9740-CC1 - All Versions
  • CM9760-CC1 - All Versions
  • CM9700-CC1 - All Versions

Cause

Failure to Identify the CM97xx-CC1 version prior to installing CM9700 System Manager may result in 9700 system failure

Resolution

  1. Connect a VGA monitor to the back of the CM9700-CC1

 

  1. In the lower right hand corner of the monitor is the version number.