How to enter the preset 95 camera menu using a CM9760-KBD keyboard.

Issue

Would like to make changes to PTZ camera settings.

Product Line

Pelco Matrix

Environment

CM9760-KBD Intelligent Keyboard

Cause

Access to the camera menu.

Resolution

Call up preset 95 procedure from CM9760-KBD

  1. First establish PTZ control with the camera
  2. Press the ESC key to open the Main menu.
  3. Press the DEF icon. The Define Submenu appears.
  4. Enter your four-digit PIN if this is your first time entering this mode.  The default pin is 1234
  5. Press the PRST icon
  6. Enter 95
  7. Press the PRST icon again.  The main menu appears on the monitor.
  8. Select the Quit icon to return to the default menu.

To program a preset, follow the instructions in Lessons Learned article "How do I program a preset from the CM9760-KBD keyboard?"