Issue
What are the different rack and wall mounts for Endura System Modules?
Product Line
Pelco Video Management
Environment
- Endura Encoder
- NET5400T
- NET5308T
- NET5308T-EXP
- NET5300B
- NET5402R-HD
Cause
Endura rack and wall mount options.
Resolution
All devices that are able to be rack mounted are supplied with rack mount kits, with the exception of the 8.75" D x 6.50" W x 1.20" H units aka the NET5301T. The following options are available for the 8.75" D x 6.50" W x 1.20" H units.
1. RK5000PS-5U Rack mount with power supply (12 units)
2. WM5200-4U Wall mount without power supply (1 unit)
3. WM5200-EXP Wall unit expansion (1 unit)
For the NET5308B, NET5308T-EXP and NET5402R-HD use the following.
4. WM5300 A WM5300 wall mount kit consists of three frames, four brackets,and 24 screws. The frames can be attached to a wall in any orientation providing a maximum of three slots.