Will the Export Viewer be on my DVD or CD when I export a video from the DX4500 or DX4600 DVR?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Using the DX4500/DX4600 Series Digital Video Recorders, is the export viewer included with a video export?

Product Line

Pelco Video Management

Environment

  • DX4500/DX4600 All Version
  • DX4500/DX4600 Export Viewer

Cause

When exporting a native clip from the DX4500/DX4600  the export viewer was not available.

Resolution

Yes, the Export Viewer is included each time you export video from the DX4500 or DX4600 DVR. This includes CD/DVD or USB.

Note: Exporting a video clip using the PC client application does not include the export viewer. The DX4500/DX4600 Export Viewer can be download here.