How to exit the DX8100 graphical user interface to Microsoft Windows Operating System.

Issue

How to exit the DX8100 graphical user interface to Microsoft Windows Operating System.

Product Line

Pelco Video Management

Environment

DX8100 Series

Cause

Configure Windows settings.

Resolution

Exit to Windows.
 
To exit the DX8100 graphical user interface and access the Microsoft Windows Operating System, perform the following:
 
1. Log into the DX8100 graphical user interface using the appropriate default credentials:
 
Default credentials for DX8100 HVR version 1.2 and lower:
Username: Admin
Password: Admin

Default credentials for DX8100 HVR version 2.0 and higher:
Username: admin
Password: admin
 
2. From the DX8100 menu bar, choose File > Exit. The Shut Down dialog box opens.
3. From the Drop-down menu, select "Exit to Windows" and click "OK". Once the DX8100 GUI has shut down, the Microsoft Windows login dialog appears.
4. Log into Microsoft Windows using default credentials:
Username: DX8100ADM
Password: dx8100
 
Note: Usernames and passwords are case-sensitive.