How to call up cameras on the DVR5100 Series using the front panel?

Issue

How to call up cameras on the DVR5100 Series front panel?

Product Line

Pelco Video Management

Environment

DVR5100 Series recorder

Cause

Bring up camera to view in the view panel.

Resolution

Follow the steps below to call up cameras from the front panel.
1.        Press the Menu button .  It will display the Main menu

 
2.        Using the Joystick, move the yellow cursor to “Cameras” on the menu item
3.        Press the Enter/Shift button to select “Cameras”. The Cameras menu appears.
4.        Using the Joystick, move the yellow cursor to “Select Camera” and press Enter/Shift. The Cameras List opens
5.        Navigate to the desired camera using the Jog (inner dial) and press Enter/Shift