Is the .ppx file that was exported from the Workstation version 2.5.9961 admissible in court?

Issue

Is the .ppx file that was exported from the Workstation version 2.5.9961 admissible in court?

Product Line

Pelco Video Management

Environment

Endura WS5000- Version 2.5.9961

Cause

Information on the acceptability of .ppx files in the court of law is needed.

Resolution

Yes. The .ppx file is a new extension for all exports from the Workstation software. The file is used as a reference when combining multiple clips into a playlist.