Issue
Need to use ASCII commands to make camera to monitor call ups.
Product Line
Pelco Matrix
Environment
CM9700 Matrix Switcher all versions
Cause
third party ASCII device needs camera control on the CM9700 Matrix.
Resolution
The ASCII string is 1Ma10#a. Where 1 is the monitor number and 10 is the camera number.