In Endura Utilities, why are some Endura NSM5200 units displayed as NSM5200 and some as NSD?

Issue

In Endura Utilities, why are some Endura NSM5200 units displayed as NSM5200 and some as NSD?

Product Line

Pelco Video Management

Environment

Endura NSM5200- All versions

Cause

For reference.

Resolution


For software version 2.02.000847 and higher. Only Members are displayed as model type “NSD”.
b. Only Managers are displayed as model type “NSM5200”.

For software version older than 2.02.000847
All Members and Mangers are displayed as model type "NSD".