What type of optical media should be used when exporting video on the DX8000 Series DVR?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

What type of optical media should be used when exporting video on the DX8000 Series DVR?

Product Line

Pelco Video Management

Environment

  • DX8000 Series DVR
  • Optical Media disc

Cause

Export video file from DX8000 to a supported optical media disc.

Resolution

Recommended media is CD-R or DVD-R, depending on which type of burner was ordered with the DX8000.