How do I hide the toolbar on the DX4100/4500/DX4600/DX4700/DX4800 Series digital video recorder?

Issue

How do I hide the toolbar on the DX4100/4500/DX4600/DX4700/DX4800 Series digital video recorder?

Product Line

Pelco Video Management

Environment

  • DX4100 Series
  • DX4500/DX4600 Series
  • DX4700/DX4800 Series

Cause

Hide the GUI toolbar on the display to prevent quick access to setup menus, dialog boxes, and controls that allow user to operate and configure the DVR.

Resolution

On the Live display, right-click the mouse on any area except the toolbar to display or hide the toolbar.

From the remote or front panel, press shift 2 to toggle OSD