Can two VGA monitors be connected to the DX4500/DX4600 Series digital video recorder?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Can two VGA monitors be connected to the DX4500/DX4600 Series digital video recorder?

Product Line

Pelco Video Management

Environment

DX4500/DX4600 Series DVR

Cause

DX4500/DX4600 Series DVR only has one VGA output.

Resolution

DX4500/DX4600 Series DVR only support one VGA video output. The DX4500/DX4600 Series DVR support the following video outputs:

  • One main VGA or analog(programming output). One at a time. Cannot be used together.
  • One analog spot (displays up to 4 cameras).