Can the CM9760-KBD Series be remote further away than the provided cables?

Issue

Can the CM9760-KBD Series be remote further away than the provided cables?

Product Line

Pelco Matrix

Environment

CM9760-KBD keyboard

Cause

Location of the CM9700-CC1 and the desire location for the keyboard are located further than the provided cables (cables are too short).

Resolution

Yes, the cable can be extended. Keep the power supply local with the keyboard by using the provided straight cable. The reversed cable from the power supply to the CM9700-CC1 can be extended up to 4000 feet (1,219 m) on 24 AWG wire.