Configure the CM9760-KBD keyboard into direct camera control mode.

Issue

  • How do I configure the CM9760-KBD keyboard into direct camera control mode?
  • CM9760-KBD direct mode

Product Line

Pelco Matrix

Environment

CM9760-KBD

Cause

Control cameras connected directly to the keyboard.

Resolution

To configure the CM9760-KBD keyboard into direct camera control mode, follow these steps:

Switch Dip Switch number 2 to the ON position to access SETUP MODE.

Enter SETUP PIN (Default: 1234)
 
  1. Select [ ADV ] from the Setup Mode Menu. The Advance Setup 1 Menu appears on the LCD display. The cursor is on the Host row.
  2. Select [ RIGHT ARROW ] to choose "Direct Cam Ctrl".
  3. Select [ DOWN FINGER ] to choose the COM port you are going to configure.
  4. Select [ LEFT ARROW ] or [  RIGHT ARROW ] to choose the baud rate and [ -I_I-I_I- ] to choose the parity.
  5. Select [ SAVE ] and then [ OPEN DOOR ] to return to the Setup Mode Menu.
  6. Select [ CAMERA ]. The Direct Camera Control Menu appears on the LCD display.
  7. Select [ LEFT ARROW ] or [ RIGHT ARROW ] to choose "Pelco" for COM 1.
  8. Select [ DOWN FINGER ] 4 times to enter the Camera Assign Menu. 
  9. Select [ DEF NUM ] to assign a logical camera number to each of the physical addresses, entrees are offset by 1.
  10. Select [ DEF NUM ]. The number is placed into the selected row for logical numbers.
  11. When you are finished configuring the last entry, select [ SAVE ].
  12. Select [OPEN DOOR] twice.
  13. Return Dip Switch number 2 back to the off position and select [OPEN DOOR].
  14. Keyboard is now in direct camera control mode.