How can the WS5200 software utilize a second monitor?

Issue

How can the WS5200 software utilize a second monitor?

Product Line

Pelco Video Management

Environment

Endura WS5200- All versions

Cause

Information regarding the usage of dual monitors on the WS5200 is needed.

Resolution

A workspace tab must be detached from the main window. Complete the following steps to detach a workspace tab.
Note:  Only 1 workspace tab can be floated at a time.
 
1.       Right click on a workspace tab
2.       Select option Float Tab. The tab will then become a separate window from the main WS5200 window.
3.       Move the float tab to the second monitor.