How do I change the DX8100 client password?

Issue

How do I change the DX8100 client password?

Product Line

Pelco Video Management

Environment

DX8100 Client software

Cause

Change the DX8100 client factory default password.

Resolution

To change the DX8100 Client password:

1. Wait while the software loads and the DX8100 Client application window opens.

2. From the DX8100 menu bar, choose File > Client Password. The DX8100 Client Password Setup dialog box opens.

3. Enter the old password in the “Old password” box. The factory default password is 000000

4. Enter a new password in the “New password” box.

5. Re-enter the new password in the “Confirm” box.

6. Click OK.

Remember the new client password or write it down and store it in a secure location.