Camclosure IS50 or IS20 series camera will not fit in a mud ring to mount it semi-flush

Issue

Camclosure IS50 or IS20 series camera will not fit in a mud ring to mount it semi-flush

Product Line

Pelco Cameras

Environment

  • IS50 Camclosure Series
  • IS20 Camclosure Series

Cause

Mud Ring for installation within or attachment to ceiling.

Resolution

You must have a mud ring that the screw holes are on a tab. There are several brands in the market place and plastic ones are available to use also. The Raco style box that goes straight across will not allow the camera to fit in it. Several companies make ones that are compatible. A few vendors and part numbers are provided in the following table.
 

Vendor Part Number
Southwire 56916501 
Hubbell 821
 
Thomas and Betts or Carlon A421 A421RR
 

Arlington Industry

 

http://www.pchcables.com/844660070191.html

 

http://www.markertek.com/Arlington-Industries-Inc.xhtml?gclid=CJK_4erS-bICFcKDQgod5H0AmA

LVS2 this is a cut in box but can be adapted by removing the locking tabs


 

Raco W2B196763