What is the thread and conduit size for the EXAC supplied gland.

Issue

What is the thread and conduit size for the EXAC supplied gland.

Product Line

Pelco Cameras

Environment

EXAC gland

Cause

Size for field installation reference

Resolution

The EXAC is provided with a liquid tight gland along the top of the enclosure. The thread size is NPT 3/4" and the conduit size is 3/4"