Error Invalid Gateway: Unable to set Static IP address for Sarix IMS0 series

Issue

Unable to set static IP address

Product Line

Pelco Cameras

Environment

IMSODN10-1

Cause

Invalid Gateway error when trying to set static IP address

Resolution

  1. Use the Network tab to change the camera's general network settings.
  2. If DHCP is set to Off, the IP address, subnet mask, gateway, and DNS server settings must be manually changed.