What is the command to restart the CM9700-CC1?

Issue

  • What is the command to restart the CM9700-CC1?
  • The CM9760-KBD is locked to a monitor and would not switch cameras

Product Line

Pelco Matrix

Environment

CM9700-CC1
CM9760-KBD

Cause

The CM9700-CC1 is at a DOS prompt or locked.

Resolution

  1. Press Ctrl Q buttons on the keyboard. DOS prompt.
  2. Confirm it's in the C:\9700 directory.
  3. Type startup  if startup does not work type CM9700 file name example: CM9700 NODE1
  4. Press Enter