How to reset the CM9760-MXB matrix bay.

Issue

The CM9760-MXB Matrix Bay needs to be reset.

Product Line

Pelco Matrix

Environment

  • CM9760-MXB Matrix Bay all versions
  • CM9760-VMC Video Monitor Card all versions

Cause

The system attributes that are displayed require updating.

Resolution

With the front panel of the CM9760-MXB removed, press the reset button located on the front of the Video Output Card (CM9760-VMC).