My IS50 and IS20-DWS ceiling template shows two different diameters for the circle to be cut. this is manual drawing C3481M.

Issue

My "IS50 and IS20-DWS ceiling template" shows two different diameters for the circle to be cut. this is manual drawing C3481M.

Product Line

Pelco Cameras

Environment

  • C3481M Manual

Cause

Manual reference of Diameter template for IS50 and IS20 cameras

Resolution

This shows 7.09 inches and in parenthesis at a different note location shows 6.3 inches. The correct value is 7.09 inches or 18.0 centimeters. This manual was corrected in August of 2011 and is now numbered C3481M-A