Recommended mounts for IS50/IS51 Camclosure 2 Series.

Issue

What are the recommended mounts for IS50/IS51 Camclosure 2 Series?

Product Line

Pelco Cameras

Environment

Camclosure 2

Cause

Mount option for Camclosure 2

Resolution

Part Number Description
IS50-P Pendant mount, outdoor; compatible with all models
IS50-CM Corner mount, indoor or outdoor; compatible with all models
SWM-SR compact wall mount, light gray finish; can be used with IS50-P for wall-mount installations; can also be adapted for corner or pole applications
WMVE-SR Wall mount, light gray; can be used with IS50-P for wall-mount installations that require increased vandal resistance or surface mount conduit
IS50-FK Flush mount kit; compatible with surface mount models only