How do I turn the WDR off on the Surevision cameras?

Issue

How do I turn the WDR off on the Surevision cameras?

Product Line

Pelco Cameras

Environment

Sarix Network Cameras with SureVision

  • IXLW Series
  • IMLW Series

Cause

To disable WDR for non wide dynamic range environments.

Resolution

You go into the menu by logging in, then do the following:

1. Click on the "settings" group
2. Under the "Imaging" pull down click on "exposure"
3. In the "exposure " menu turn flicker correction to on.

This turns the WDR to off.