Power supply kit for remote powering a KBD300A Keyboard.

Issue

What is the power supply kit for remote powering a KBD300A Keyboard?

Product Line

Pelco Matrix

Environment

KBD300A keyboard
KBDKIT (120 VAC to 12 VAC 200mA)
KBDKIT-X (230 VAC to 12 VAC)

Cause

Convert 120 VAC to 12VAC to power up KBD300A.

Resolution

The part number for remote powering a KBD300A Keyboard is KBDKIT.

The Remote Keyboard Wiring Kits of the KBDKIT Series are used to connect KBD100, KBD200 or KBD300 keyboards to the CM6700, CM6800 and CM9700 Matrix Switchers.

The KBDKIT in addition can be used to connect the KBD4000 keyboard to the Genex™ MX4000SVR Multiplexer Server or Genex™  MX4000 Series Multiplexer.

The kits are also used when installing either the KBD200 or KBD300 for Direct Mode control of Pelco receivers.

Models

  • KBDKIT         Remote keyboard wiring kit that includes two RJ-45 wall blocks and a transformer to convert 120 VAC power to 12 VAC 200mA for keyboard power.
  • KBDKIT-X     Remote keyboard wiring kit that includes two RJ-45 wall blocks and a transformer to convert 230 VAC power to 12 VAC for keyboard power.

Click link to download manual KBDKIT Series Manual.

Note: KBDKIT's Transformer Power Input: 120V 60Hz 9W.  Power Output: 12VAC 200mA