Instant Recording on the DX8100 Series hybrid video recorder (HVR)

Issue

  • How to stop Instant Recording on the DX8100 Series hybrid video recorder (HVR)
  • Timeline display black bars instead of blue or green

Product Line

Pelco Video Management

Environment

DX8100 Series HVR

Cause

Disable the Instant Recording mode to disable the manually start and stop a video recording session instantly.

Resolution

To stop instant recording:

  • Double-click the Instant Recording icon (CD symbol) located in the lower-right corner of the view pane of the camera in question.

    Verify the instant recording icon changes from blue to silver, indicating that instant recording is de-activated.

Note: Must be logged in to get the instant record feature.