What are the CM9760-CXTA coaxitron translator dip switch settings for controlling Spectra cameras from a device using D protocol?

Issue

What are the CM9760-CXTA coaxitron translator dip switch settings for controlling Spectra cameras from a device using D protocol?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • CM9760-CXTA
  • Pelco D
  • Pelco P

Cause

The CM9760 CXTA switch settings allow the CXTA to receive commands in RS422 D or P protocol and convert the commands into coaxitron to control the PTZ camera.

Resolution

  1. On the CM9760-CXTA turn on dip switches 3 (D Protocol), 5, 6 (2400 Baud Rate) and 8 (Spectra) and power cycle the unit. 
  2. This will set the CM9760-CXTA to accept D protocol commands at 2400 baud with parity none.
  3. For P Protocol and additional settings see the CM9760-CXTA Manual Page #11.