Where is the current version of software the CM9760-CC1 / CM9700-CC1 is running displayed?

Issue

Software version of the CM9760-CC1 / CM9700-CC1 is required.

Product Line

Pelco Matrix

Environment

  • CM9760-CC1 all versions
  • CM9700-CC1 all versions

Cause

The current software version is required in order to match correct Pelco System Manager.

Resolution

It is displayed in the lower right hand corner of the diagnostic VGA monitor connect to the CM9760-CC1 / CM9700-CC1.