Spectra camera is stuck in the camera setup menu and will not exit.

Issue

When the Spectra camera is stuck in the camera setup menu and will not exit, can it be powered off and then back on to clear the camera menu?

Product Line

Pelco Cameras

Environment

Spectra Analog Series

Cause

  • 95 Preset Menu is displaying and does not allow exit of menu
  • Navigation of Menu is not allowed.
  • Communication to Camera has failed during menu access

Resolution

Power Down the Spectra camera, then power back on to clear the camera menu; the camera settings will be preserved.