What type of cable is recommended to remote the CM9760-KBD keyboard?

Issue

What type of cable is recommended to remote the CM9760-KBD keyboard?

Product Line

Pelco Matrix

Environment

  • CM9700 Matrix Switcher all versions
  • CM9760-KBD Intelligent Keyboard all versions

Cause

Keyboard is to be installed in a remote area which exceeds the factory cable lengths.

Resolution

Cat5e or equivalent should be used when installing the CM9760-KBD keyboard in a remote location.