What are the recommended mounts for the IE Series Sarix IP?

Issue

What are the recommended mounts for the IE Series Sarix IP?

Product Line

Pelco Cameras

Environment

Sarix IE Series

Cause

Mounting options for Sarix

Resolution

Recommended Mounts:
 

Part Number Description
IE-P Pendant mount adapter, light gray
IE-S Surface mount adapter, light gray
SWM-SR* Wall mounts, light gray
IWM-SR* Wall mounts, light gray
PP350* Parapet mount, gray
PP351* Rooftop or horizontal surface mount, gray
IWM24-SR* Wall mount with cable feedthrough; includes integral 24 VAC, 100 VA transformer; light gray finish

*Requires the IE-P pendant mount adapter.

NOTE: click on the part number for product specification