How to connect the CM9760-KBD keyboard to the CM9760-CC1 / CM9700-CC1

Issue

How is a CM9760-KBD keyboard connected to a CM9760-CC1/CM9700-CC1?

Product Line

Pelco Matrix

Environment

  • CM9760-KBD keyboard
  • CM9760-CC1
  • CM9700-CC1

Cause

Install the CM9760-KBD for a full-function desktop keyboard that allows users to control matrix systems.

Resolution

The following steps also apply to connecting a CM9760-KBD keyboard to CM9740-CC1, CM9760-CC1, CM9700-CC1, CM9760-CDU-T, CM9760-CXTA, CM9760-MDA or CM9760-DMR.

  1. Make sure all DIP switches are OFF
  2. Connect the RJ-45 straight cable from the COM 1 port on the CM9760-KBD keyboard to the keyboard connector on the power supply.
  3. Connect the RJ-45 reversed cable from the System connector on the power supply to the input port on the CM9740-CC1, CM9760-CC1, CM9700-CC1, CM9760-CDU-T, CM9760-CXTA, CM9760-MDA or CM9760-DMR. Note: The Maximum distance is 4000 feet for RS422/485
  4. Plug in the power supply.
  5. Turn the main power supply switch ON.

 

Instructions were taken from the CM9760-KBD Installation / Operation Manual , on page 13.