What is the maximum number of Genex Multiplexers that can be added to a CM9760-CC1/CM9700-CC1 sercom port?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Multiple Genex Multiplexers are required per sercom port.

Product Line

Pelco Matrix

Environment

  • CM9700 Matrix Switcher version 7.80.029 and up
  • Genex Multiplexer any version

Cause

Limited number of sercom ports available.

Resolution

Up to 16 Genex Multiplexers can be added per sercom port with a 5 sercom port maximum for a total of 80.