Resolution supported for composite input for the PMCL542NB monitor

Issue

What is the resolution that is supported on composite input for the PMCL542NB monitor

Product Line

Pelco Monitors

Environment

  • PMCL542NB

Cause

Analog resolution value

Resolution

The PMCL542NB monitor supports the Resolution of 720X480 with Vertical Frequency 30 HZ and it can not be changed.  The mode supported is SDTV 480i.