DX4100 Series Main BNC Output video display is blank or scrambled?

Issue

DX4100 Series Main BNC Output video display is blank or scrambled?

Product Line

Pelco Video Management

Environment

DX4100 Series

Cause

Dip switch setting.

Resolution

For the Main BNC Output to function, ensure the Rear-Panel Dip-Switch is set to TV.

1. Locate the S/W (switch) on the rear of the DX4104. See figure 1, #14 for the S/W switch.

2. Set the switch to the up position (TV). The position enables main monitor output to the main out BNC connector.

3. Reset power to the unit.
 

 


Figure 1. DX4104 Rear-panel