Does the DX8100 PC Client require a Microsoft Windows user account with administrator/admin privileges

Issue

Does the DX8100 PC Client require a Microsoft Windows user account with administrator/admin privileges

Product Line

Pelco Video Management

Environment

DX8100 PC Client

Cause

The DX8100 client user can not add a new site or change the settings in the DX8100 client program.

Resolution

Yes

The DX8100 PC Client is not a Microsoft Windows multiuser application, the Microsoft Windows user must have full write access to the install folder.