How is the NUIconf.niu file copied to a CM9700-NW1 network interface unit using a 3.5 inch floppy disk?

Issue

Need to load a NUIconf.niu file to a CM9700-NW1.

Product Line

Pelco Matrix

Environment

  • CM97000-NW1
  • 3.5" floppy disk

Cause

Current file is out dated.

Resolution

  1. On the CM9700-NW1 network interface unit press CTRL+Q to exit the 9700nui application.
  2. Insert the floppy disk into the A: drive.
  3. At the DOS prompt C:\NETWORK> type:
    copy a:*.niu
  4. Press ENTER, to copy the file.
  5. To restart the CM9700-NW1 application type:
    net Press ENTER
    or
    9700nui NUIconf.niu Press ENTER