Keyboards compatible with the CM9760-CXTA coaxitron translator when using direct camera control.

Issue

Which Keyboards are compatible with the CM9760-CXTA coaxitron translator when using direct camera control?

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • CM9760 Keyboard Series
  • KBD300A (with KBDKIT)
  • KBD200A (with KBDKIT)

Cause

Desktop controller for connection to CM9760-CXTA

Resolution

The CM9760-KBD, CM9760-KBR, KBD200A and KBD300A keyboards are all compatible.
The CM9760 keyboards will use P protocol while the KBD200A/300A keyboards operate in D protocol.

 

Note: KBD300A, KBD200A series require the addition of the KBDKIT product.