Issue
Are the CM9760/70/80-VCC video input cards hot swappable?
Product Line
Pelco Matrix
Environment
- CM9740-MXB all versions
- CM9760-MXB all versions
- CM9765-MXB all versions
- CM9770-MXB all versions
- CM9780-MXB all versions
Cause
Replace or reseat a Video Camera Card.
Resolution
Yes. You do not need to power off the Matrix Bay or CM9700-CC1 to remove an input card.
Must be same model of Video input card for example
- CM9760-VCC is compatible with CM9760-MXB, and CM9740-MXB.
- CM9765-VCC is compatible with CM9765-MXB.
- CM9770-VCC is compatible with CM9770-MXB.
- CM9780-VCC is compatible with CM9780-MXB.