Are the video CM9760/70/80-VCC video input cards slot specific?

Issue

Are the video CM9760/70/80-VCC video input cards slot specific?

Product Line

Pelco Matrix

Environment

  • CM9760-VCC Video Input Cards
  • CM9770-VCC Video Input Cards
  • CM9780-VCC Video Input Cards
  • CM9760-MXB Matrix Bay
  • CM9770-MXB Matrix Bay
  • CM9780-MXB Matrix Bay

Cause

Not sure how to address the Video Input Cards.

Resolution

No. The input cards can occupy any of the available slots; you can also hot swap input cards for trouble shooting purposes.