How do I change the video input termination on the DVR5100 hybrid video recorder?

Issue

How do I change the video input termination on the DVR5100 hybrid video recorder?

Product Line

Pelco Video Management

Environment

DVR5100 Series HVR

Cause

Disable video termination for video to loop out.

Resolution

By default, the video termination on the DVR5100 is set to 75 ohms.  To change the video termination follow these steps:

  1. Log in to the DVR5100 using an administrative level user.
  2. Press the "M" key on the keyboard [or Menu button] to display the Main menu.
  3. Click on Setup to display the setup screen.
  4. Select the Cameras tab. The cameras screen appears.
  5. Choose desired camera from the camera list.
  6. Uncheck the box "Video termination" which allow for video to loop out of the DVR5100
  7. Apply changes and exit.