Programming a preset in the DX4500/DX4600 Series DVR

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How to program a PTZ camera preset on the DX4500/DX4600 Series DVR

Product Line

Pelco Video Management

Environment

  • DX4500/DX4600 Series DVR
  • Spectra PTZ positioning system

Cause

Preset settings were not program.

Resolution

Programming a Preset

  1. On the front panel or remote control, press any of the arrow buttons    to select a PTZ camera pane. Using the mouse, click
    a camera pane.
  2. On the front panel or remote control, press PTZ. Using the mouse, click the PTZ button  . The PTZ control is displayed.
     
  3. Position, zoom, and focus the camera.
    On the front panel or remote control, press any of the arrow buttons   to move the camera. Using the mouse, click the Move buttons  .
    On the front panel, press SHIFT + ZOOM or remote control, press ZOOM. Using the mouse, click ZOOM.
    On the front panel, press SHIFT + FOCUS- or FOCUS+. On the remote control, press FOCUS. Using the mouse, click FOCUS.

     
  4. Store the preset to a memory location.

    On the front panel, press SHIFT + SET or remote control, press SET. Using the mouse, click SET. The camera is now in the programming mode.
    On the front panel or remote control, press a number representing the preset memory location. Using the mouse, click a number on the keypad. On the front panel, press SHIFT + PRESET.
    On the remote control, press PRESET. Using the mouse, click PRESET. The camera’s position, zoom factor, and focus setting are stored to the memory location.

     
  5. Do one of the following:

    To create multiple presets for the same camera, repeat steps 3 and 4.
    To exit the programming mode, on the front panel, press SHIFT + SET. On the remote control, press SET. Using the mouse, click SET.

     
  6. Verify that you can activate the preset. 
    On the front panel or remote control, press any of the arrow   buttons to move the camera to another location. Using
    the mouse, click the Move buttons  . 

    If you changed the camera’s zoom or focus, verify that the settings are different than the preset settings. 
    Do one of the following: 
                         On the front panel, press the preset number, and then press SHIFT + PRESET
                         On the remote control, press the preset number, and then press PRESET
                         Using the mouse, click the preset number, and then click PRESET.


    The camera performs the programmed preset. The camera performs the programmed preset.